|
 |
|
01.Why my UPS will not turn on?
The on/off switch is designed to prevent damage by rapidly turning it off and on. Please turn the UPS off. Wait 10 seconds and then turn the UPS on. |
| |
02.Why the outlets do not provide power to equipment?
Please check first whether the fuse is blown due to overload. If yes, turn the UPS off and unplug at least one piece connected equipment. Unplug the power cord of the UPS then remove the fuse compartment beneath the power inlet of the UPS and replace the blown fuse with a spare one. Lock the compartment back to the UPS. Connect power cord then turn the UPS on. Make sure that your spare fuse meets the specification: 6.3A, 250V, 5x10mm.
If the fuse is normal, the possible cause might be that batteries are discharged. Please Allow the unit to recharge for at least 4 hours.
|
| |
03.Why UPS will switch to battery mode (using battery led illuminate) then switch back when I turn on it?
The UPS will execute self-test automatically when turned on. This mechanism is to make sure the total load is within the nominal capacity.
|
| |
04.Why can't I cold start my UPS?
The UPS will execute self-test automatically when turned on. This mechanism is to make sure the total load is within the nominal capacity. |
| |
05.When utility power recover, why my computer protected by UPS can not auto restart itself?
If your computer is of ATX type, you should change the setting in BIOS to allow auto restart when utility power recovers. |
| |
06.The equipment plugged into the UPS doesn't accept RS232 signal but only the contact closure signal. Why can't I use contact closure function in Cyber Power Office series UPS?
The contact closure function is disabled out of factory. You can down the S/W patch to enable the contact closure function. |
| |
07.How can I connect the UPS with a USB cable?
Please connect the enclosed serial interface cable to the serial port on the UPS and an open serial port on the computer. If you would like to use USB interface, please connect the USB adapter with the Serial Cable then connect the USB to your computer.
|
 |
| |
08.Where is the serial number located on the unit?
The serial number is located on the back panel underneath the bar code. The serial number will has total 12 numbers. For example: EC14Z2000010. You would use the serial number for registration purposes.
|
| |
09.My CyberPower unit is beeping. Why?
CyberPower units have a feature called "Sensitive to on line voltage". This detects quick changes that occur in the AC voltage. These changes are within the safe operating range of the unit. When these occur, the UPS switches to battery power to keep the voltage constant.
This feature can become disruptive with the unit beeping frequently. If it does, the sensitivity feature will need to be turned off.
Turning off the Sensitivity feature.
- Click on the battery icon near the time display in the lower right corner of the screen.
- Click on Setup.
- The first line in the setup screen is labeled "Sensitive to variation online voltage."
- Uncheck the box to the left of this line.
- Click the OK button.
- Minimize the display by clicking on the green minimize bar under the power button.
- Shutdown the computer.
- Turn the CyberPower unit off.
- Wait 15 seconds.
- Turn the unit back on. The unit will beep three times during a self-test.
- Restart your computer
|
| |
10.The power failed and my equipment shut off, what is wrong (Utility series)?
Check to be sure that you have the computer and the monitor plugged into the battery power supplied outlets. There are two sets of three outlets on the unit. Three provide battery power and three provide surge protection only
|
| |
11.I am not getting any power from the battery outlets, what should I do?
Attempt to reset the unit by doing the following:
- Turn the unit off.
- Unplug everything from the unit.
- Leave the CyberPower unit plugged into the wall socket.
- Wait 15 seconds. Turn the unit back on.
- Three short beeps will indicate the unit doing a self-test.
- Test the battery powered outlets with a low wattage item such as a 60 Watt lamp.
|
| |
12.I don't have an available serial port, will my CyberPower UPS work without the software?
The use of the PowerPanel/PowerPanel Plus software is not necessary for the successful operation of the unit. Your computer will not shutdown automatically unless you are using the software. For further information about different connection options, please contact CyberPower directly.
|
| |
13.What outlets should I plug my equipment into?
Your computer and monitor need to be plugged into the battery power supplied outlets. If you have an externally powered data storage device (tape drive, Zip drive, etc? that should also be plugged into the battery outlets.
Other devices such as scanners, printers and speakers, should be plugged into the surge protection only outlets. Items such as laser printers, vacuums, curling irons and space heaters MUST NOT be plugged into the unit at all. Doing so will overload the unit and void your warranty. |
| |
14.How do I configure the UPS function supplied by NT to monitor my CyberPower UPS unit?
The use of the NT UPS service is optional. NT provides a "generic" UPS monitoring System that can be used in place of PowerPanel/PowerPanel Plus. You can only use One UPS monitoring program at a time.
Make sure that PowerPanel/PowerPanel Plus is either removed or not running. Set the UPS function signals to:
- Power Failure Signal: Negative
- Low Battery Signal: Negative
- Remote UPS Shutdown: Positive
- Select the correct COM port to start the UPS service
|
| |
15.What is the surge response time of a CyberPower UPS?
Instant |
| |
16.Why does the approximate backup time show in red?
The approximate backup time can show in one of three colors: green, yellow, or red. The colors are based on the number of minutes available. For example, if the approximate backup time shows in red, you have less then 10 minutes available. |
| |
17.How do I run a self-test?
There are two types of self-tests that can be run on the unit. The first involves use the software, and the second simulates a power failure.
To run the software test:
- Open the PowerPanel/PowerPanel Plus screen.
- Click the setup button
- Click the red run button
This test switches the unit to battery for 5 seconds. The unit will beep during this self-test.
To run the power failure simulation test:
- Make sure that the battery is fully charged.
- Unplug the unit from the wall
- The unit will beep while it is unplugged.
- Please note that the UPS will turn off 2 minutes after the software starts to shutdown the computer. If you plug in the UPS before the UPS shuts down, the UPS will not restart and will not provide power to the battery outlets. To correct this, turn the UPS off, wait 10 seconds and then turn the UPS on.
|
| |
18.What UPS Characteristics ?
- Provide clean and consistent power
- Protect systems against spike and surge
- Supply battery backup power
- Shut down computer safely
- Avoid data loss and hardware damage
|
| |
19.What UPS Applications ?

|
| |
| |
| |
| |